EEO#.LINES
Description
Sets how many lines are output for one revolution of the source feedback. When configured to output CW/CCW or step/dir signals (EEO#.MODE 1 or 2) you will get 4 times this value of pulses per revolution.
Examples
Code
This will set the number of EEO2 lines to 8096.
-->EEO2.LINES 8096
Context
For more information see Output - Encoder Emulation.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | N/A |
| Range | 0 to 16777215 |
| Default Value | 1024 |
| Data Type | Integer |
| See Also | |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.